Effects of Upgrading - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Upgrading a CAF to a new Release mode enables you to load new firmware for the device and configure features available with the new firmware. The upgrade also has the benefit of updating standard modules.

After you have upgraded, unique preferences for system selection, common object naming, and default controllers are preserved. The current release mode of your application is displayed in both the status bar and the application title bar.

For further information see: