Backup Files - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

When you upgrade your system, the tool creates a backup version of the original file and stores the file in the same directory as the original file. The backup file has the same name as the original file; however, the backup file has a .bak extension. To use the backup file, you need to remove the extension from the file name.

Note: The default location of a CAF is C:\Users\username.