Monitored Safeties (UV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Discharge Air Smoke Detector and Low Limit Temperature Switch selections create optional Sensor points that can be mapped to the Supervisory system and alarm points created.

The selection options for Monitored Safeties are:

  • Discharge Air Smoke Detector

  • Low Limit Temperature Switch