Economizer Suitability (UV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Economizer Suitability selections are not available when ASHRAE Cycle 1 is selected. Otherwise, the Economizer Availability Determination Setpoint module is created and interfaced to the choice selected.

The selection options for Economizer Suitability are:

  • Network Command

  • Binary Input (Enthalpy Switch)

  • Outdoor Air

    • Dry Bulb Temp Economizer

    • Temp & Enthalpy Economizer