Transfer to Computer (Upload) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

You can transfer to a computer using the Transfer Wizard. You are able to discover available devices or manually specify a device address.

While it is possible to use the Transfer to Computer feature on an unlicensed device, the uploaded CAF will be set to Artificial Field Device.