Connections - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English
The Supervisor Passthru connection mode allows you to select a Metasys® NAE through which to connect to perform the operation.
Note: You do not need to launch the tool through the supervisory device configuration tool or user interface, or have the supervisory device configuration tool installed to use the Supervisor Passthru connection. When the tool is launched from the supervisory device configuration tool, the supervisory device connection information is not automatically populated in the tool.

To use an Supervisor Passthru connection, enter the device host name or IP address, your user credentials, and click Login.

The Bluetooth connection mode allows you to select a local Bluetooth card or a Bluetooth Wireless Commissioning Converter to connect through to perform the operation.

The MAP 4.2+ / BACnet Router connection mode allows you to select a MAP 4.2+ / BACnet Router to connect through to perform the operation.

The ZigBee connection mode allows you to select a local ZigBee USB dongle to connect through to perform the operation.

The Direct Ethernet connection mode allows you to easily connect directly to an IP device.