The following table describes the attributes used by the Staged Device Enable Determination Series module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Fan Mode |
Indicates whether the fan is currently commanded on. |
Off Set Name: Off/On |
|
Staged Device Min Flow |
Indicates the minimum required flow before issuing a command to true without the fan being commanded on. |
100.0 | 200.0 Display Units: l/s | cfm |
|
State |
G |
Provides the desired status to Staged Enable. |
False Set Name: False/True/Fault |
Supply Flow |
Indicates the measured supply flow. |
0.0 Display Units: l/s | cfm |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)