Attributes (Unoccupied Sequencing [VAV]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the VAV Unocc Status Determination modules.

Table 1. Unoccupied Sequencing (VAV) Attributes

Name

Description

Default Value

Box Heating Control Status

Used to indicate to this module that it can affect the box heating output.

Overridden

Set Name: Control Status

Cooling Setpoint

Desired unoccupied cooling temperature setpoint.

28 °C, 82 °F

Detailed State

Contains the detailed unocc state giving devices requested.

Set Name: VAV Unocc Detailed

Heating Priority

Indicates which heating to use first when both box and supplemental heating exist.

Supplemental

Set Name: VAV Heating Priority

Heating Setpoint

Desired unoccupied heating temperature setpoint.

16 °C, 61 °F

Occupancy

Contains the current Occupancy mode as determined by Occupancy Mode Determination.

Occupied

Set Name: Occ Effective

State

Current state of the hybrid activity.

Set Name: Unoccupied Status States

Supp Heating Control Status

Used to indicate to this module that it can affect the supplemental heating output.

Overridden

Set Name: Control Status

UNOCC-SATTIME (Satisfied Timer Duration)

Time that the Zone Temperature must be within the limits before switching to Satisfied.

30 Seconds

UNOCC-STATE (Unocc Status)

Contains the current unoccupied status.

Set Name: VAV Unocc Status

See Primary States (Unoccupied Sequencing [VAV]).

WarmupCooldown

Current WarmupCooldown State.

Normal

Set Name: OST Warmup Cooldown

Zone Temperature

Current Zone Temperature.

22 °C, 72 °F