Unoccupied Sequencing (VAV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This module generates an Unocc Status for the VAV applications. When not in Unoccupied, the Unocc Status is Unocc Cntrl Not Req’d which allows other sequencers to control the devices. When unoccupied and Warmup or Cooldown are active, the Unocc Status is Unocc Cntrl Not Req’d. When unoccupied and Warmup and Cooldown are not active, the zone temperature is monitored to determine when the temperature exceeds the band specified by the two unoccupied temperature setpoints. When this occurs, the Unocc Status is set to the appropriate heating or cooling state. The module remains in this state until the appropriate setpoint has been satisfied for the Satisfied Timer Duration. After that period of time the status is set to Satisfied.

When unoccupied, if the temperature is unreliable, the Unoccupied Status is set to Temperature Unreliable.

For information on how the FSM determines the state, see FSM (VAV Unoccupied Sequencing).