Attributes (Last Value) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Table 1 describes the attributes used by the State Generation Last Value (Boolean, Enum, Float) modules.

Table 1. Last Value (Boolean, Enum, Float) Attributes

Name

Type 1

Description

Default Value

Input

 

Passes the Default Value to the Present Value on the first execution after startup or enable. Otherwise the Current Value of the Input is passed to the Present Value.

False

1st Enum

0.0

Present Value

G, V

Output of this module.

 
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)