The following table describes the attributes used by the Unit Enable Determination modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Hardware Mode |
Specifies whether to allow the unit to operate normally or to shutdown. |
Enable Set Name: Shutdown/Enable |
|
Network Mode |
Specifies whether to allow the unit to operate normally or to shutdown. |
Enable Set Name: Shutdown/Enable |
|
PFRESTART-EN (Power Fail Restart Enable) |
Specifies that, when this value is set to true, a timer holds the output at shutdown until the Power Fail Restart Time elapses. |
False |
|
PFRESTART-TIME (Power Fail Restart Time) |
Specifies that, when the power fail restart logic is enabled, the start is delayed by the time specified in this value. |
60.0 Seconds |
|
Resolution Mode |
Used when both inputs are connected to determine how the two input commands (network and hardware) should be resolved into a single output command. |
Either Can Shutdown Set Name: Resolution Mode2 |
|
UNITEN-STATE (State) |
G, V |
Current desired state for the unit. |
Set Name: Shutdown/Enable |