Attributes (System Mode Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The following table describes the attributes used by the System Mode Determination modules:

Table 1. System Mode Determination Attributes

Name

Type 1

Description

Default Value

Eff Mode

G, V

Indicates the effective System mode after splitting off the Water Flush output.

Set Name: Effective System Mode

System Mode

 

Indicates the current System Mode.

Auto

Set Name: System Mode

Water Flush

V

Indicates whether Water Flush is requested.

Boolean

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)