The Effective Occupancy is determined based on four inputs: Occupancy Schedule, Occupancy Sensor, Temporary Occupancy, and Occupancy Override.
The Occupancy Override has the highest priority in the Decision Table. If the Occupancy Override is Occupied, Unoccupied, or Standby, the Effective Occupancy is set to that value. The Occupancy Override can also be set to Bypass or Not Set. When the Occupancy Override is set to Bypass, it does not directly set the Effective Occupancy, but may trigger the Bypass Timer as described as follows.
The Bypass Timer has the second highest priority in the Decision Table, but is allowed to operate only if the Occupancy Schedule is not equal to Occupied (that is, it is equal to Standby, Unoccupied, or Not Set). The Bypass Timer is reset if the Occupancy Schedule becomes equal to Occupied and is prevented from restarting as long as the Occupancy Schedule remains equal to Occupied. The Bypass Timer also is reset if the Occupancy Override is set to a value other than Bypass or Not Set.
When the Occupancy Schedule is not equal to Occupied, if either the Occupancy Override is Bypass or if the Occupancy Override is Not Set and the Temporary Occupancy input is Active, the Bypass Timer is started for the Bypass Time. When active, the timer restarts when the Occupancy Override is Not Set and the Temporary Occupancy input changes from Inactive to Active or when the Occupancy Override changes from Not Set to Bypass. The Bypass Timer is allowed to continue timing if the Occupancy Override is set to Not Set.
The Bypass Time is user configurable. If the Bypass Timer is active and the Bypass Time is changed, the Bypass Timer is restarted for the new Bypass Time.
The Occupancy Schedule has the third highest priority in the Decision Table. If the Occupancy Schedule is Unoccupied or Standby, then the Effective Occupancy is set to that value. If the Occupancy Schedule is Occupied but the Occupancy Sensor indicates no one is present (that is, value is Unoccupied), then the Effective Occupancy is set to Standby to conserve energy. Otherwise, the Effective Occupancy is set to Occupied.
The Occupancy Sensor has the lowest priority in the Decision Table. If the Occupancy Schedule is Not Set, the Occupancy Sensor directly sets the Effective Occupancy. Finally, if all of the inputs are Not Set and the Bypass Timer is False, then the effective Occupancy Mode is set to the Default Occupancy property (initially equal to occupied).
Occupancy Override (Supervisory Override Command) |
Temp Occupancy (Bypass Timer) |
Occupancy Schedule (Supervisory Command) |
Occupancy Sensor (Hardware Sensor) |
Effective Occupancy (Effective Occupancy Result) |
---|---|---|---|---|
Occupied |
* |
* |
* |
Occupied |
Unoccupied |
* |
* |
* |
Unoccupied |
Standby |
* |
* |
* |
Standby |
Bypass or Not Set 1 |
True |
Occupied 2 |
* |
Occupied2 |
NOT Occupied 3 |
* |
Bypass |
||
False |
Occupied |
Occupied |
Occupied |
|
Not Set1 |
Occupied |
|||
Unoccupied |
Standby |
|||
Unoccupied |
* |
Unoccupied |
||
Standby |
* |
Standby |
||
Not Set1 |
Occupied |
Occupied |
||
Unoccupied |
Unoccupied |
|||
Not Set1 |
Default Occupancy 4 |