Occupancy Mode Determination (MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This module extends the base Occupancy Mode Determination module with support for a Temporary Occupancy input for up to eight zones (with the zone number designated here by X, representing zones 1-8). You can view and modify this module; however, you cannot change the key behavior performed by the Occupancy Mode Determination module.