Attributes (Fan Alarm Status) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the Fan Alarm Status modules.

Table 1. Fan Alarm Status Attributes

Name

Type 1

Description

Default Value

Fan Alarm

G, V

Indicates if a fan alarm has been detected.

 

Fan Mode

 

Contains the current fan command.

Off

Set Name: Off/On

Flow Status

 

Current status from the Air Flow Status module.

False

Set Name: False/True/Fault

Reset

 

Used to clear the Fan Alarm and allow the fan to restart.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)