The state output is generated from the Network mode and Hardware mode inputs based on the Resolution Mode setting. The following table shows the command hierarchy used to determine whether the State should be Normal or Energy Hold Off.
Resolution Mode |
Network Reliable |
Network Mode |
Hardware Reliable |
Hardware Mode |
State |
---|---|---|---|---|---|
Network Priority |
True |
Normal |
* |
* |
Normal |
Energy Hold Off |
* |
* |
Energy Hold Off |
||
False |
* |
True |
Normal |
Normal |
|
Energy Hold Off |
Energy Hold Off |
||||
False |
* |
Normal |
|||
Hardware Priority |
* |
* |
True |
Normal |
Normal |
Energy Hold Off |
Energy Hold Off |
||||
True |
Normal |
False |
* |
Normal |
|
Energy Hold Off |
False |
* |
Energy Hold Off |
||
False |
* |
False |
* |
Normal |
|
Either Can Activate |
True |
Normal |
False |
* |
Normal |
True |
Normal |
Normal |
|||
Energy Hold Off |
Energy Hold Off |
||||
Energy Hold Off |
* |
* |
Energy Hold Off |
||
False |
* |
True |
Normal |
Normal |
|
Energy Hold Off |
Energy Hold Off |
||||
False |
* |
Normal |