Application Mode Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

AHU applications have an Application Mode input that allows you to force the unit into a mode of operation. The possible modes are Cool Only, Heat Only, Fan Only, Water Flush, Purge, Vent, and Auto. This module separates the Water Flush mode to a separate output to allow it to be separately connected to State Selection.

You can view and modify the modules in this group’s logic.