Primary States (Occupied Zone Sequencing [VAV]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English
  • Satisfied: The sequencer is in this state when Heating or Cooling are not needed.

  • Supp Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint and Box Priority = Supplemental.

  • Supp Htg + Box Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Supplemental, and Supp Heating Control Status = High.

  • Box Heating: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint and Box Priority = Box.

  • Box Htg + Supp Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Box, and Box Heating Control Status = High.

  • Prmy Clg: The sequencer is in this state when the Zone Temperature is greater than the Cooling Setpoint.

  • Temperature Unreliable: The sequencer is in this state when the Zone Temperature is not reliable.