Occupied Zone Sequencing (VAV) HFR - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

This module determines if the box should be in the heating flow reset (HFR) mode or the standard modes (non-HFR module). The State Table is set up to manage the HFR mode correctly along with the HFR output controller(s). This module generates the appropriate temperature control state for a VAV zone control application. This module monitors the status of the heating and cooling controllers and setpoints to determine whether the current state should be satisfied, unreliable, one of the stages of heating, or one of the stages of cooling. This module uses a heating flow reset strategy that increases flow when the maximum heating output is reached. For information on how the FSM determines the state, see FSM (Occupied Zone Sequencing [VAV] HFR).

This module also provides a quick transition from heating to cooling mode during major changes to space load conditions or setpoints (for example, a large group of people enter a space, or a schedule changes from unoccupied to occupied mode).