The following table describes the attributes used by the Occupied Sequencing (AHU MASD w HR) module.
Name |
Description |
Default Value |
---|---|---|
AHU-STATE (State) |
Represents the current state generated by the sequence. |
Satisfied |
Cooling Control Status |
Value fed back from the mechanical cooling PID controller necessary for the sequencer to determine what actions to take. |
Normal Set Name: Control Status |
Cooling Setpoint |
Contains the setpoint the state generator attempts to control when cooling. |
13 °C, 55 °F |
Damper Control Status |
Value fed back from the economizer PID controller necessary for the sequencer to determine what actions to take. |
Normal Set Name: Control Status |
Fan Ready |
Comes from the Start/Stop Sequencer and indicates that the fans and dampers have been sequenced properly. |
False |
Fast Sequence Enabled |
Indicates whether a change to a Satisfied state occurs when a setpoint changes as described in the Setpoint Threshold input. |
False |
Free Cooling Available |
Contains the output of the Economizer Availability module. |
False |
Heat Recovery Control Status |
Contains the value fed back from the heat recovery PID controller necessary for the sequencer to determine what actions to take. |
Normal Set Name: Control Status |
Heat Recovery Modulated |
Indicates whether the heat recovery is modulated, where True equals modulated and False equals not modulated. |
False |
Heating Percent Cmd |
Indicates the current command from the heating controller that operates first. This signal comes directly from the PID in the output controller module. |
0.0 Display Units: % |
Heating Setpoint |
Contains the setpoint the state generator attempts to control when heating. |
13 °C, 55 °F |
Preheat Control Status |
Contains the value fed back from the preheat PID controller necessary for the sequencer to determine what actions to take. |
Normal Set Name: Control Status |
Preheat Percent Cmd |
Indicates the preheat command used to prevent the preheat from cycling off and on unnecessarily when the AHU starts. |
0.0% |
Process Variable |
Contains the value compared to the setpoint and is used to determine whether heating or cooling is required. |
13 °C, 55 °F |
Reheat Control Status |
Value fed back from the reheat PID controller necessary for the sequencer to determine what actions to take. |
Normal Set Name: Control Status |
Setpoint Threshold |
Indicates how much the Cooling Setpoint must increase/Heating Setpoint must decrease to cause a change to a Satisfied state from a Cooling/Heating state. |
1 °C, 2 °F |
Zone Control |
Contains a Boolean input that is True when the unit is Zone Control without Cascaded DA-T setpoint reset. |
False |