Input |
Behavior When Input Is Not Reliable |
---|---|
Duct Static Pressure 1 |
If both Duct Static Pressure 1 and Duct Static Pressure 2 inputs are unreliable, a shutdown Sequence is initiated. |
Duct Static Pressure 2 |
If both Duct Static Pressure 1 and Duct Static Pressure 2 inputs are unreliable, a shutdown Sequence is initiated. |