Module Use in Applications (Start Stop Sequencing [AHU Mixed Air]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Start Stop Sequencing (AHU Mixed Air) Uses in Application System Selection Trees

Module Instance Name

Applications

Start Stop Sequencing

AHU Mixed Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

Start Stop Sequencing DA-T

AHU Mixed Air Single Duct Applications(DA-T Control)

AHU Rooftop Unit Applications

Start Stop Sequencing Zone

AHU Mixed Air Single Duct Applications (Zone Control)

AHU Rooftop Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.