Attributes (PID Tuning Reset) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the PID Tuning Reset modules.

Table 1. PID Tuning Reset Attributes

Name

Type 1

Description

Default Value

Application Tuning Reset

 

Provides a trigger to reset the tuning parameters of the PIDs in the output controllers.

False

PID Tuning Reset

 

When set to True, signals the output controllers to calculate new tuning parameters instead of controlling.

False

State

 

Provides the state to feed through State Selection to place the output controllers in the appropriate State Selection section to allow recalculation of the PIDs tuning parameters.

Set Name: PID Tuning Reset

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)