The following table describes the attributes used by the Heat Recovery Low Limit Sequencing module.
Name |
Description |
Default Value |
---|---|---|
Delay |
When Heat Recovery Modulated is False, this input defines the amount of time the Low Limit Temperature must be greater than the Low Limit Temperature Setpoint before the unit can return to the T Control state. |
120 Seconds |
Heat Recovery Control Status |
Contains the value fed back from the output controller PID. This is needed for the sequencer to determine what actions to take. |
Normal Set Name: Control Status |
Heat Recovery Modulated |
Contains a configuration input used to tell the state machine if the heat recovery is modulated or not. True means modulated, and False means not modulated. |
False |
HRLL-STATE (State) |
Represents the current operational mode of the state generator. |
T Control |
Low Limit Process Variable |
Contains the value that is compared to the limit setpoint and used to determine whether it is necessary to switch from T Control to LL-T Control. |
4 °C, 39 °F |
Low Limit Setpoint |
Contains the limit setpoint used to determine whether it is necessary to switch from T Control to LL-T Control. |
4 °C, 39 °F |