Analog Override Check - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The Analog Override Check module checks multiple signals to determine whether the outputs associated with them are overridden. This module is used within a Control Sequence.

The Analog Override Check module monitors the priority of output objects. The Number of Input Attributes property sets the number of objects monitored by this module. When any input is overridden and the Setup value is OR, the output is set to True. When all inputs are overridden and the Setup value is AND, the output is set to True.