Pass Through (Device Enable) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The Device Enable Pass Through modules provide an automatic connection to the State Selection module. They typically take Network Inputs and connect them to State Selection. The Device Enable category’s Pass Through modules have the same configuration as the Pass Through category’s Pass Through (Boolean, Enum) module.