Module Use in Applications (Heat Recovery Suitability Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the name in the following table.

Table 1. Heat Recovery Suitability Determination Uses in Application System Selection Trees

Heat Recovery Suitability Determination

Applications

Heat Recovery Suitability Determination

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.