Reliability (Heat Recovery Enthalpy Suitability Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Heat Recovery Enthalpy Suitability output is set to None if the OA Temperature, Exhaust Air Temperature, or the Low Limit Process Variable inputs are not reliable.