Attributes (Secondary Bypass Valve Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by this module.

Table 1. Secondary Bypass Valve Sequencing Attributes
Attribute Type 1 Description Default Value
Low Limit Enable  

Indicates the desired setpoint of the PID Pct Cmd. When PID Pct Cmd falls below this setpoint, and if the system is enabled, the output switches to True.

0.0%
PID Pct Cmd   Represents the variable to which the Low Limit Enable setpoint is compared. 0.0%
State   Indicates the current operating mode of module. False
System Enable   Enables the process to run using a True/False command. False
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)