Secondary Bypass Valve Sequencing - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This module is responsible for controlling the state of the secondary bypass valve PID, based on system enable and the output of the secondary pumping PID. This module is implemented as a standard Control Activity.

Figure 1. Secondary Bypass Valve Sequencing Module