Plant Sequencing-Discrete - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Plant Sequencing-Discrete module is responsible for sequencing pumps, interlocks, and stages of a discrete plant system to maintain a setpoint. This module accepts as inputs a process variable, a setpoint, a deadband, a heating/cooling flag, a Stabilize Delay, an Up Delay, a Down Delay, a Number of Devices Running, a System Interlock Status, a Start-Up Delay, Minimum Running Devices, and a System Enable. Based on the input commands and the attribute settings, the module outputs a state for sequencing pumps, interlocks, and stages of a discrete plant system and an output for the number of devices to run.

You can view and modify the modules in this group’s logic.