Module Use in Applications (Plant Sequencing-Decouple) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Plant Sequencing-Decouple Uses in Application System Selection Trees

Module Instance Name

Applications

Chiller Sequencing by Decouple Loop Flow

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.