Attributes (Load Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The following table describes the attributes used by the Load Calculation modules:

Table 1. Load Calculation Attributes

Name

Type 1

Description

Default Value

Flow

 

Indicates the rate the media is moving through the system.

0

Display Units: l/s, gpm

Glycol Concentration

 

Indicates the percentage of Glycol in the system.

0

Display Units: %

HeatingCooling

 

Switches the Load output, so a positive value is output for either a Heating or Cooling Mode.

Heating

Set Name: Heating/Cooling

Load

V

Indicates the calculated Load.

0

Display Units: W, Btuh

Media

 

Indicates the type of media used in the system.

Water

Set Name: Load Media

Return Temperature

 

Indicates the temperature of the media returning from the system.

0

Display Units: °C, °F

Supply Temperature

 

Indicates the temperature of the media supplied to the system.

0

Display Units: °C, °F

Unit Set

 

Switches the calculation based on the application’s system of units.

IP

Display Units: SI, IP

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)