Attributes (Device Enable Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The following table describes the attributes used by the Device Enable Determination modules:

Table 1. Device Enable Determination Attributes

Name

Type 1

Description

Default Value

Device Enable n

 

Establishes the enable status of the device. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.)

True

Enable n Out

G

Contains the enable value (Boolean) for the corresponding Device. (Where n is 1-8.)

True

Iso Vlv A Enable n

 

Establishes the enable status of an isolation valve. A Boolean value of False takes the associated device out of service. If a device is on when this input is set to False, Enable n Out is set to False immediately. (Where n is 1-8.)

True

Iso Vlv B Enable n

 

Establishes the enable status of a second isolation valve. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.)

True

Pump A Enable n

 

Establishes the enable status of a pump. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.)

True

Pump B Enable n

 

Establishes the enable status of a second pump. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.)

True

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)