Attributes (Count On Inputs) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The following table describes the attributes used by the Count On Inputs modules:

Table 1. Count On Inputs Attributes

Name

Type 1

Description

Default Value

Input #

 

Indicates if the device status is off or on. Input # is a Binary input.

Off

Limit Variable

 

Acts as a high limit in the number of devices that are able to run. Limit Variable is a floating value.

8

Output (Float)

V

Indicates the current number of devices that are ON.

0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)