Count On Inputs - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
This module is responsible for determining if any of the interlock devices are on. The module accepts eight status inputs as well as a limit input value that acts as a high limit. Based on the input commands and the parameter settings, the module outputs the number of devices that are ON.

You can view and modify the modules in this group’s logic.