Module Use in Applications (Central Heating Low Temp Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Central Heating Low Temp Control Uses in Application System Selection Trees

Module Instance Name

Applications

Frost Protection Determination

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.