The following table describes the attributes used by the Condenser Water Sequencer modules:
Name |
Description |
Default Value |
---|---|---|
Bypass Control Status |
Indicates the current control status of the bypass valve control. This input typically comes from the bypass valve control module. This provides appropriate timing to prevent cycling between modes. |
Normal Set Name: Control Status |
Condenser Water Setpoint |
This is the setpoint to which the condenser water is being controlled. |
21 °C, 70 °F |
Condenser Water Temperature |
This is the process variable. |
21 °C, 70 °F |
Delay |
This input is the delay time to wait to enter the tower control state from the bypass valve control state after the bypass valve PID reached 100%. |
180 Seconds |
OA Humidity |
This input is the outdoor air humidity. |
50% RH |
OA Temperature |
Outdoor air temperature. |
21 °C, 70 °F |
State |
Shows current state of this output controller. |
Off Set Name: Condenser Water |
Switchover Diff |
This is the differential used to prevent cycling as the outdoor air wetbulb floats around the switchover setpoint. |
2.5 °C, 5 °F |
Switchover Setpoint |
This is the setpoint this module uses to determine if the outdoor air wetbulb is too warm to provide control of the condenser water with only the bypass valve. If the OA Humidity is unreliable or not connected, the module uses only the OA Temperature. |
21 °C, 70 °F |
System Enable |
Indicates when the chilled water system is enabled. |
True |
Tower Control Status |
Indicates the current control status of the cooling tower control. This input typically comes from the cooling tower PID control module. This provides appropriate timing to prevent cycling between modes. |
Normal Set Name: Control Status |