Commanding Network Inputs and Network Outputs - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

About this task

Note: System simulation is paused when you transition into Edit mode or open a Command dialog box. Simulation immediately resumes when you exit the window.

Procedure

  1. Right-click a Network Input or Network Output and select Commands.
  2. Enter the Test value or select Restore to restore the value to the default.
  3. Click OK. The Commands details dialog box appears with the Test value in the Details area.
  4. Select Enable or Disable.
  5. Click Send to send the command and close the dialog box, or click Cancel to close the dialog box without sending the command.