Commanding Items - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

About this task

Note: For steps on commanding Network Inputs or Network Outputs, see Commanding Network Inputs and Network Outputs.
Note: System simulation is paused when you transition into Edit mode or open a Command dialog box. Simulation immediately resumes when you exit the window.

Procedure

  1. Right-click an item that can be viewed and modified and select Commands. The right-click menu appears.
  2. Select the Attribute from the Attribute drop-down menu.
  3. Click the browse button next to Attribute Command to open the parameter or attribute’s specific command dialog box.
  4. Do one of the following:
    1. Select Test, enter a test value for the command, and click OK.
    2. Select Restore to restore the value to the default and click OK.
    3. Click Cancel to cancel the command.
    The Command details appear in the Details area of the dialog box.
  5. Click Send to issue the command and close the dialog box. Or, click Cancel to close the dialog box without issuing a command.