Break Conditions Detail Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

See the Working with Break Conditions section.

Table 1. Break Condition Details Dialog Box
Field Description
Variable Indicates the break condition object or attribute.
Criteria The standard by which the Value is measured.
Value Indicates the break condition threshold value.
Enabled

Indicates if the break condition is enabled.

Note: When a break condition appears during a simulation, the user has the option to click Disable in the dialog box that appears. If the user clicks Disable, then the Enable check box is cleared.

Add Break Condition

Saves and closes the Break Condition Details window.

Update Break Condition

Saves the updated break condition and closes the Break Condition Details window.

Cancel

Closes the window without applying the changes.

Opens the Help system.

Note: The Active icon () is only visible in the Break Condition Detail dialog box when the break condition has been reached through system simulation.