Position Feedback (Sideloop) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The selection options for Position Feedback are:

  • Modulated Outputs
    • No Position Feedback
    • Analog Input per Output
    • Binary Input per Output
  • Two Position Outputs
    • No Position Feedback
    • Binary Input per Output
    • Two Binary Inputs per Output