Importing Localization Preferences - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Procedure

  1. On the desired tab of the Preferences - Localization screen, click Import. The Open dialog box appears.
  2. Select the localization properties file to import.
    Notes:
    • The default file name for each tab is listed in the Import and Export Preferences section.
    • You may need to browse to the location where you saved the file if you saved it to a different location from the default or received the file from others.
  3. Click Open. The preferences file opens and populates the Preferences - Localization screen.