Procedure
- Click Export. The Save dialog box appears.
-
Keep the default file name of ObjectNaming.properties or adjust the name to indicate a specific site or use.
Note: It is not necessary to export/save a separate copy of the Johnson Controls standard preferences because the Reset and Reset All functions reset the preferences to the Johnson Controls standard default values regardless of user session.
-
Keep the default location to save the file or adjust it as desired.
Note: The default location is C:\ProgramData\Johnson Controls\MetasysIII\<Product Name>\Configuration\Backup\Object Naming
- Click Save. The file saves and you can access it from the same computer for later use or you can copy the file to use on another computer.