Unit Preferences - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

You can set the units of measurement to use when working in the tool from the New System dialog box (File > New) during the System Selection process. After setting the units and closing the tool, the tool remembers the last unit’s setting. The selected units are used until you change them in the New System dialog box. See Selecting a System (Creating a New System) in the Configuring a System section.