Reliability (Sideloop Minimum Selector) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Table 1. Sideloop Minimum Selector Reliability

Input

Behavior When Input Is Not Reliable

Input 1

The last Reliable value is used in the minimum selection.

Input 2

The last Reliable value is used in the minimum selection.