Reliability (Sideloop Maximum Selector) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Table 1. Sideloop Maximum Selector Reliability

Input

Behavior When Input Is Not Reliable

Input 1

The last Reliable value is used in the maximum selection.

Input 2

The last Reliable value is used in the maximum selection.