Attributes (Sideloop Maximum Selector) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Table 1 describes the attributes used by the Sideloop Maximum Selector modules.

Table 1. Sideloop Maximum Selector Attributes

Name

Type 1

Description

Default Value

Input 1

 

Contains the first input used to determine the maximum.

0.0

Input 2

 

Contains the second input used to determine the maximum.

0.0

Present Value

G, V

Maximum of the inputs.

 
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)