This module selects the maximum value of the inputs to produce the output. The module accepts two inputs and outputs the maximum of the inputs. The user can add more inputs to the module.
You can view and modify the modules in this group’s logic.
To see this module’s connections and how modules interact with it:
-
view the Connection table. For details, see Connections in the Perspectives section and Viewing and Modifying Connections in the Configuring a System section.
-
view the Show Involvement dialog box. For details, see Showing and Hiding Involvement in the Commissioning a System section.