Table 1 describes the attributes used by the Sideloop Average Inputs modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Input 1 |
Contains the first input to be averaged. |
0.0 |
|
Input 2 |
Contains the second input to be averaged. |
0.0 |
|
Present Value |
G, V |
Average of the inputs. |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)